System Default Calibration

The Default System Calibration creates a system cal for TDR, GDM, and other uses. This adjustment is for service only; not for measurement calibration.

Required Equipment

DC ECal or Mechanical Calibration Kit

See VNA Accessories

 

Notes

  • You must be logged onto the VNA as an Administrator to perform an adjustment. Learn more.

Procedure

  1. Click Utility, then System, then Service, then Adjustment Routines...

  2. At the Adjustments selection, click System Default Calibration. The System Default Calibration dialog is displayed as shown below.

  3. Select the calibration method (ECal or Mechanical Standards).

  4. Click on the Begin Cal button to begin the calibration.

  5. Follow the instructions displayed in the program.

Data Storage