IF Gain Adjustment


This adjustment sets the IF attenuator/gain stages to present a relatively consistent level to the ADC versus frequency for a given amount of signal.  This maximizes the dynamic range of the instrument by preventing any IF compression at higher levels.  The adjustment range is about 18dB with one adjustment value per band per input:  R1, R2, R3, R4, A, B, C, and D (if applicable.)

The program first finds the peak of each band’s frequency response with a fixed input level. It then re-measures those peaks with a power meter.  From this information, it determines the optimum gain or attenuation needed to keep all bands as similar as possible for any given frequency.

When to perform

IF Gain Adjustment should be performed when any of the following occur:

Required Equipment

Procedure

Note: You must be logged onto the VNA as an Administrator to perform an adjustment. Learn more.

Click Utility, then System, then Service, then Adjustment Routines...

At the Adjustments selection, click IF Gain Adjustment.

Note: Connect the Power Meter/Sensor to the VNA USB, GPIB, or LAN input depending on the type of Power Meter/Sensor being used. The program will prompt you where and when to attach the RF input for the Power Sensor(s).

Ensure the Reference Channel paths are properly configured and the connections are properly torqued.

  1. Click Begin

  2. Follow the instructions displayed in the program.

The adjustment takes about 5 minutes to complete for a 26.5 GHz VNA. Higher frequency units may take longer.

The Default menu selection (under the advanced menu) is for factory personnel only. This will preset all values to default levels for trouble shooting purposes only. If this is selected, a full IF gain adjustment will need to be performed.

Data Storage