The following Tools, Utilities, and Adjustments are available to help you keep your VNA at peak performance.
Not all of the adjustments listed below are valid for every VNA model. Only the adjustments needed for each particular VNA will be listed.
To access the service adjustments on the VNA, click Utility, then System, then Service, then Adjustment Routines...
Standard Adjustments
TDR Adjustments
10 MHz Reference Frequency Adjustment
Source Adjustment
Receiver Adjustment
IF Response Adjustment (applies ONLY to instruments with serial prefix 6021 and above with A.14.00.xx firmware and above.)
When a Millimeter mode is detected, the following adjustments are displayed.