IF Gain Adj for mm Mode

This program adjusts the gain of the IF mux in the N5290A/91A system.

This adjustment is for service only; not for measurement calibration.

Required Equipment

See list of supported power meters and sensors.

See VNA Accessories

 

Notes

  • You must be logged onto the VNA as an Administrator to perform an adjustment. Learn more.

Procedure

  1. Click Utility, then System, then Service, then Adjustment Routines...

  2. At the Adjustments selection, click IF Gain Adj for mm Mode. The PNA IF Gain Adjustment for Wideband dialog is displayed as shown below.

  3. Select the first port to adjust. Each port with a frequency extender connected must be adjusted.

  4. Click on the Begin button and follow the instructions displayed in the program.

  5. Set up the power sensors then click OK. Up to three different power sensor configurations can be saved and recalled.

  6. Follow the instructions displayed in the program.

Data Storage