This program adjusts the source and receiver of the N5293AX03/N5295AX03 Frequency Extenders.
This adjustment is for service only; not for measurement calibration.
See list of supported power meters and sensors.
See VNA Accessories
Notes
|
Click Utility, then System, then Service, then Adjustment Routines...
At the Adjustments selection, click Source and Receiver Adj. The PNA Src/Rcvr Adjustment dialog is displayed as shown below.
Select the first port to adjust. Each port with a frequency extender connected must be adjusted.
Click on the Begin button and follow the instructions displayed in the program.
Follow the instructions displayed in the program.
The correction data is stored in the flash memory.