Clicking Project
in the tree view displays the Projected Waveform table
in the parameter view of
the main window.


This cell displays the waveform name. It is automatically generated when you enter the Project Name in the left pane. You cannot edit this cell.
This cell displays the projected file length in the number of data points for each waveform. The number of data points is calculated as follows:
[Data Points] = [Sampling Clock] * [Frame Duration] * [Built Frames].
It changes automatically as you enter the Frame Duration and Built Frame data in the left pane. Increasing the oversample ratio increases the number of data points. The maximum number of data points a waveform can have depends on your signal generator option.