Installation Steps: 1 2 3 4 5 6 7 8 9
Visit the Software Download web page.
Click the button. Select a version of the executable to download, and install the software onto your PC.There are 32 bit and 64 bit versions of the application. Windows XP and Win 7 32 bit use the 32 bit version. Win 7 64 bit requires the 64 bit version. At the prompt, select Run to install the software directly, or select Save to save a copy of the installation software on your PC.
The N7620B software must be installed with administrator privileges. For Windows XP, you must be logged in as administrator. For Windows 7, right-click the installer and select Run as administrator.