Installation Steps: 1 2 3 4 5 6 7 8 9
After starting the N7620B software, the
Configuration
Wizard
is used to configure the I/O interface for the signal generator, arbitrary
waveform generator, and spectrum/signal analyzer.
Turn on the equipment and, if necessary, the computer.
If using an external Arbitrary Waveform Generator (M8190A, M9330A, N6030A, or N8241A), turn on the Arb and verify correct functionality using the
instrument's soft front panel or control utility.
Start the software.
Establish communications between the software and the
equipment by first selecting in the
Welcome
to Keysight Signal Studio for Pulse Building
dialog box (System Configuration Wizard) that appears.
Select a
hardware
configuration
from the list (Wideband I/Q, External I/Q, or Internal Arb) then click
.
Use the configurations that do not include a signal analyzer only if you do not plan to use signal corrections.
Select
<New>
and click .
Enter the GPIB or LAN address
for the
signal generator.
To find the signal generator's LAN information, (IP address/hostname), press the following front panel keys:
Utility > GPIB/RS-232 LAN > LAN Setup.
To find the signal generator's GPIB address, press the following front panel keys:
Utility > GPIB/RS-232 LAN > GPIB Address.
Click the
button to automatically check the
I/O connection
of the signal generator. Click
to continue.
Enter the GPIB, LAN or PXI address for the
external arb.
The N603xA/M933xA Control Utility can be run to determine the PXI address of the Arb. The addresses of all N603xA/M933xA Arbs found in the system can be viewed in the by looking in the menu.
Click the
button to automatically check the
I/O connection
of the external arb. Click
to continue.
Enter the GPIB or LAN address for the
spectrum/signal analyzer.
Click Next to automatically check the
I/O connection
of the analyzer. Click to
continue.
Enter a
system
name
and click Finish to save the current setup.
After making the connections you can view the
system's information
by selecting from the drop-down
menu.
Install the software license.
Run Self Test to make certain the system is configured correctly.
If the connection fails, or for help with error messages, refer to Troubleshooting.