This menu item clears calibration data from the signal generator's memory. Clearing the calibration data allows new data to be written to the signal generator. Clearing calibration data is recommended, but not required, if the calibration data is older than 24 hours.
Use Generate Correction to replace a single entry in the calibration data base. Use Clear Calibration Data to clear the entire data base.