Verifies the active pattern, creates the pattern signal data (including the waveform, sequence and marker data), applies corrections, downloads the signal to the signal generator's volatile waveform memory and sets up signal generator settings associated with the baseband signal and turns on the Arb. The signal generator will automatically play the signal. The selection uses the Advanced settings to configure a signal. Refer to the Advanced Command Button section for more information.
You can manually save the signal to the signal generator's non-volatile waveform memory. In addition, you can save the signal generator parameters and settings, configured in the Advanced setting section, to one of the signal generator's save/recall registers. Recalling the register will set up signal generator parameters to play the signal with the correct settings.
Only the internal Arb supports saving waveform data to non-volatile memory.