Advanced Pattern Details

The Advanced button provides access to pattern-specific functionality. It is possible to design several patterns, each with its own specific setup, such as a different frequency and amplitude while also having a different trigger mode. The Compact button closes the Advanced Pattern Details window and returns to the compact mode.

For details about each parameter, click a topic name under Advanced Pattern Details in the Help window's Contents pane.

Each downloaded signal contains waveform and sequence data for the arbitrary waveform generator as well as settings for the signal generator. Many of the signal generator values may be updated by simply pressing the play button. Switching between patterns that have been downloaded is accomplished by selecting the desired pattern from the pattern list and pressing play.

The waveform and sequence data downloaded to the PSG/MXG/EXG/ESG internal Arb is placed in volatile memory. The data may be copied to non-volatile memory for permanent storage. Use the instrument save/recall feature to save the other instrument settings for this signal. When you want to play a previously stored waveform, load the waveform into volatile memory and recall the associated instrument state. Refer to the Download section for more information.

Pattern Library Overview

Pattern Details

Menu Bar and Toolbar