This is the phase difference of the carrier phase of a pattern item relative to the carrier phase of another pattern item. If only one pattern item defines a pattern then the phase offset is relative to the carrier.
Phase
Offset can be entered in either radians or degrees. To control whether
degrees or radians is used, select
Phase Offset
in radians
or
Phase Offset in degrees
in the Customize
Pattern Item Table.