View

The View menu consists of the following menu items: 

These menu items are used to change the appearance of the Pulse Building application's main form. You can select how the interface is presented, what forms (pulse library or pattern library or both) and what parameters you want visible in the pattern library table.  

Pattern Library

This menu item displays the Pattern Library form.

Pulse Library

This menu item displays the Pulse Library form.

Both Libraries

This menu item displays both the Pulse and Pattern Library forms.

Customize pattern item table...

This menu item displays the Custom Pattern Detail Tableform. This form, shown below, lists all available pattern parameters using the column titles that appear on the Pattern Details table. You can select which parameters you want to be visible on the table by placing a check in the desired parameter check box. The customized table changes only how the pattern item table appears. Though unselected parameters do not appear on the table, they are not disabled and are still used by the software to calculate the baseband signal. Also, you can still enter values for parameters located on the Pattern Details Antenna and PRI panels, even if they do not appear on the table.

The Select Column Preset provides choices of pre-selected sets of parameters to appear on the Pattern Details table. The figure below shows the Default choice with all parameters selected. The column preset choices include the following:

Selecting Phase Offset in radians or Phase Offset in degrees controls Phase Offset in the Pattern Details table.