Play Test Signal

The test signal is a multitone signal that contains 20 tones with staggered frequencies (so the images are readily seen). The bandwidth of the test signal is set with the Signal Bandwidth parameter. See Test Signal Image Reduction.