CSV Files Introduction

The CSV file format contains all of the Pulse Building application properties for a single pattern. It does not, however, contain hardware-specific configuration properties like those found under the Download menu.

To import an existing CSV file containing pattern data, click the File > Import Pattern menu item. To export pattern data to a CSV file, click the File > Export Pattern menu item. The simplest way to generate a template for a CSV pattern file is to create a new pattern in the Pattern Library with several different objects in it and then export it. Then you can modify the file to re-import later.

An example CSV file and supporting files are installed with the Pulse Building application. Review the files to see how a CSV file is organized. The example is available at:

Windows 7

C:\Users\Public\Public Documents\Keysight\Pulse Building\Samples\csv_example

Windows XP

C:\Documents and Settings\All Users\Keysight\Pulse Building\Samples\csv_example

CSV File Format

CSV File Importation Rules

CSV File Exportation Rules

Import Pattern...

Export Pattern...