The Object group contains the following properties:
|
Object_Type |
|
Object_Name |
|
Off_Time_us |
|
Repeat |
The Object properties are organized as shown in the
example pattern items under Object, appearing in the columns after the Index header. The properties in this section include the object type to generate, the object name, the off time in us, and the number of times to repeat the object. Valid objects include pulses, patterns, and off time. When the object type is off, all other values in the row are ignored except for the Off_Time_us, which is used for the off time length. If the object type is Pattern, an empty pattern is created unless a pattern with the specified name already exists in the Pattern Library.
The Index item is shown with the Object group since it is located in the first column immediately preceding the group. The index value is ignored. It is provided as a visual aid when creating pulse patterns in CSV files.