The RF Offsets group contains the following properties:
|
Freq_Offset_MHz |
|
Power_Scale_dB |
|
Phase_Offset_Deg |
The RF Offsets properties are organized as shown in
example pattern items under RF Offsets. These properties are offsets that are applied to the RF output using I/Q modulation. The offsets include Frequency Offset, Phase Offset, and a Power Scale. The offsets for a given line are relative to objects in other lines as well as to the RF frequency and the RF amplitude. The offsets are applied to all objects specified by the number of repetitions. The offsets are additive, so if the Power Scale is set to -10 dB, and an antenna scan is applied to 1000 pulses, the amplitude for each pulse produced by the antenna patterns is reduced by 10 dB. With the Power Scale set to 0 dB, the maximum possible amplitude from the antenna pattern is 0 dB.