2. Output (M8190A)

Go to topic Go to description Go to topic Go to topic Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description

Channel 1/2

Accesses the properties for this channel. The properties for channel 1 and channel 2 are identical.

Clock Source

Double-click or use the drop-down menu to select the channel clock source.

Channel 1 and Channel 2 sample clock sources are coupled when channel coupling is enabled.

The N7621B software sets Channel 1 to Internal and Channel 2 to External when configured in "Arb Only" Mode.

Output Mode

Double-click or use the drop-down menu to select the channel output mode.

Channel 1 and Channel 2 output modes are coupled when channel coupling is enabled.

Switching the output mode clears existing waveforms from memory.

Direct Mode

Double-click or use the drop-down menu to select the channel direct mode.

Channel 1 and Channel 2 direct modes are coupled when channel coupling is enabled.

Switching the direct mode clears existing waveforms from memory.

Interpolated Mode

Double-click or use the drop-down menu to select the up sampling ratio used in interpolation mode.

The I/Q data is automatically up sampled to match the DAC sample rate. Using a larger interpolation reduces the amount of I/Q data needed but also reduces the signal bandwidth.

Channel 1 and Channel 2 interpolated modes are coupled when channel coupling is enabled or when channel 1 and channel 2 share the same clock source.

DAC Format

Double-click or use the drop-down menu to select the DAC format.

Output Route

Double-click or use the drop-down menu to select the channel output route.

The AC and DC path share common output connectors on the front panel. The direct DAC path uses different connections on the front panel.

Output State

Double-click or use the drop-down menu to enable or disable the current output. The current output is determined by the "Output Route" property.

Compliment Output State

Double-click or use the drop-down menu to enable or disable the current complement output. The current complement output is determined by the "Output Route" property.

Output Voltage

Range:

Direct DAC: 200 mV to 1.40 V (peak to peak differential)

DC Output: 300 mV to 2.00 V (peak to peak differential)

AC Output: 200 mV to 2.00 V (peak to peak)

Set the peak to peak output voltage.

The Output Voltage and IQ Gain Balance properties are coupled.

See also: Carrier Scale and Output Route

Output Voltage Offset

Range:

Direct DAC: -20 mV to 20 mV

DC Output: -500 mV to 1.0 V

AC Output: Not Applicable

Set the output offset voltage.

The full voltage offset range is coupled to the current Output Voltage and the Output Route values.

Differential Offset

Range: -8192 to 8191

Set the differential amplitude offset in DAC values.

Termination Voltage

Range: -1.0 V to 1.0 V

Set the DC gain termination voltage.

Fine Delay

Range: 0 ps to 30 ps

Set the fine channel delay relative to a trigger or event.

The fine delay, I/Q Skew and Trigger Delay are coupled.

Course Delay

Range: 0 ps to 10 ns

Set the course channel delay relative to a trigger or event.

The course delay, I/Q Skew and Trigger Delay are coupled.

Carrier Scale

Range: 0.0 to 2.83

Set the carrier scale. The carrier scale is used to prevent clipping of the digital data by the DAC. The digital up conversion (DUC) process can generate values that exceed the DAC range. Clipping is prevented by setting the carrier scale to less than the maximum value. The software resets carrier scale to 2.0. This is 70% of the maximum value. Adjusting the carrier scale directly affects the signal output power and dynamic range. Larger values are better until clipping occurs.

Only available when the software is configured in "Arb Only" Mode.

See also: Amplitude

Carrier Frequency Integral

Range: 0 to 12 GHz

Set the integral part of the carrier frequency.

Only available when the software is configured in "Arb Only" Mode.

Carrier Frequency Fractional

Range: 0.0000 to 1.0000 Hz

Set the fractional part of the carrier frequency.

Only available when the software is configured in "Arb Only" Mode.