Band Power measures the input carrier band power, output carrier band power, and band power gain of the DUT (magnitude and phase).
In this topic:
The procedures in the list below must be performed prior to making Band Power measurements. For purposes of this example, the DUT used is an amplifier and the Modulation Type is Flat Tones.
The Sweep, RF Path, Modulate, or Measure tab functions can now be selected.
Select the Measure
tab.

In the Measurement Type pull down menu, ensure that Band Power is selected (default).
Click on the Autofill button to automatically fill in the measurement settings for all bands from the currently active modulation file loaded in the source. Therefore, changing the settings in the following steps is optional.
To offset the Carrier integration bandwidth relative to the Carrier LO used to generate the modulation signal, use the up/down arrows in the Carrier Offset Freq field or double-click in the field then enter the value using the displayed keypad.
To set the Carrier integration bandwidth for the distortion measurement, use the up/down arrows in the Carrier Integ BW field or double-click in the field then enter the value using the displayed keypad. The IBW is used to determine total signal power within a specified frequency span.
To adjust
other measurement settings, click on the Measurement
Details... button:

To set the frequency span window used for modeling the DUT's gain and distortion, use the up/down arrows in the Distortion Measurement Correlation Aperture field or double-click in the field then enter the value using the displayed keypad. Checking Auto will automatically set Distortion Measurement Correlation Aperture to window size.
To select the IF filter anti-aliasing path, click on the ADC Anti-alias Filter pull down menu then select Auto, Wide, or Narrow. Auto will automatically set the ADC Filter setting based on the ADC Sampling Frequency. If the currently selected modulation waveform was created with Nyquist Rejection = OFF, then the VNA will measure the signal using the Narrow anti-alias filter in the receiver. Wide selects the ADC 38 MHz IF filter path. Narrow selects the ADC 11 MHz IF filter path. A warning message will appear if the Narrow IF filter path is selected and the Resolution Bandwidth is > 1 MHz.
To set the measurement filter to either None (default) or RRC (root-raised-cosine filter), click on the Modulation Filter pull down menu then make the selection. With RRC selected, Alpha sets the Alpha factor of the filter and Symbol Rate sets the Symbol Rate of the filter. If Auto is selected, the Symbol Rate from the file is used. If no Symbol Rate is indicated in the file, then the Symbol Rate will be approximated from the bandwidth of the signal.
Click on the OK button.
Click on the Apply button to apply the setting changes made in this dialog.
Click on the OK button to close the dialog.
Ensure that the VNA Trigger is set to Continuous. Press Trigger > Main > Continuous.
The Distortion
Table is displayed below the measurement area. Each column represents
a measurement parameter. The measurement parameters shown in the Distortion
Table below are the default parameters selected for a Band Power measurement.

The measurement
parameters are selected using the Distortion
Table Setup dialog. To add or change parameters, press Meas
> Main > Distortion Table... or
right-click on the Distortion Table displayed below the measurement
area then select Edit Columns...
in the pop-up menu. The Distortion
Table Setup dialog is displayed:

Check the desired measurement parameters then click on the OK button.
To view a trace displaying the Input/Output Band Power and Band Power Gain, perform the following:
Press
Meas > Main
> Other... then
click on the "..."
button. The Measure
dialog is displayed:

Select the Distortion
tab to display distortion traces:

Check CarrIn1 to measure input Band Power then click on the Apply button.
In the Distortion tab, check New trace. If any parameters are currently checked, uncheck them.
Check CarrOut2 to measure the output Band Power then click on the Apply button.
In the Distortion tab, check New trace. If any parameters are currently checked, uncheck them.
Check CarrGain21 to measure the Band Power gain then click on the OK button.
If necessary, press Scale > Main > Scale Coupling..., select Window as the Coupling Method, then click OK. This re-scales all traces to the same scale.
Click on the Autoscale All softkey.
The
following is an example of a typical trace and Distortion Table showing
input and output Band Power and Band Power Gain: