Limited Port Mapping


The IMD, IMDx, IMSpectrum, and IMxSpectrum Apps have a limited port mapping capability. This would allow you, for example, to simultaneously measure two 2-port DUTs in different channels.  You could input the 2-tone signal to port 1 and port 3. The DUT output would be connected to port 2 and port 4.

Port selections are made on the Power Tab for each Application.

Note: This setup requires an external combiner connected to the rear-panel. The external combiner that is shown has two inputs and two outputs. This can also be accomplished by using two components.

This example setup shows a 4-port transceiver connected to the VNA ports as follows:

VNA Port

DUT Port

1

Rx In

2

Rx Out

3

Tx In

4

Tx Out

Notes

Programming Commands