IM Spectrum for Amplifiers (Opt S93087A/B)


Intermodulation Spectrum measurements can be made independently, or coupled with Swept IMD measurements. They are a distinct measurement class. Therefore, IM Spectrum measurements are always made in a separate channel.

Note: This feature is not available for PNA-X Pro.

See Also


Limitations with IM Spectrum

The following VNA features are NOT available in an IM Spectrum channel:

Create an IM Spectrum Channel

An IM Spectrum channel can be created independently from a Swept IMD channel or coupled with the stimulus settings of an existing Swept IMD measurement.

To create an independent IM Spectrum channel

  1. Press Meas > S-Param > Meas Class....

  2. Select IM Spectrum, then either:

To create an IM Spectrum channel from an existing Swept IMD channel

  1. With a Swept IMD channel active, press Marker on the front panel.

  2. Move the marker to the data point of interest. It can be moved later.

  3. Press Marker > Marker Functions > Marker -> IM Spectrum.

This creates or configures an existing IM Spectrum channel based upon the configuration of the Swept IMD channel.

To perform this function remotely:

Execute the VBScript file located on the VNA.

  1. Create a macro. Either send this command or it can be done manually:
    SYST:SHOR10:PATH “C:\Program Files (x86)\Keysight\Network Analyzer\Applications\IMD\imd.vbs”

  2. Execute the macro using: SYST:SHOR10:EXEC or the equivalent COM command: Execute Shortcut Method

Notes:

  • 10 is the macro number. If you are already using this number for a macro, it will be overwritten.

  • The marker must already be on the IMD trace and be the active marker.

  • The path name to imd.vbs may be different on your VNA.

 

Select IM Spectrum Parameters

How to add IM Spectrum traces

With the IM Spectrum channel active and a Tr1 Output trace displayed:

Using Hardkey/SoftTab/Softkey

Using a mouse

  1. Press Trace, then select trace.

  2. Press Meas, then select a parameter.

  1. Click Instrument, Trace, Add Trace.

  2. Click Response, Meas, then select a parameter.

Programming Commands

New Trace - IM Spectrum -dialog box help

Choose from:

  • Output Spectrum  View signals OUT of the DUT and into VNA port 2 (B receiver).

  • Input Spectrum  View signals IN to the DUT (R1 receiver). Use this when measuring IM product frequencies to determine the power level of spurious signals into the DUT at those frequencies.

  • Reflection Spectrum  View signals reflected off the DUT input and back into VNA port 1 (A receiver)

IM Spectrum Setup Dialog

How to start the IM Spectrum Setup dialog   

With an IM Spectrum measurement active:

Using Hardkey/SoftTab/Softkey

Using a mouse

  1. Press Sweep > Main >  IMS Setup....

  1. Click Stimulus

  2. Select IMS Setup...

Programming Commands

Frequency tab - IM Spectrum -dialog box help

Note: The number of data points in an IM Spectrum channel = 3 * SPAN / ResBW. This can NOT be changed directly.

Configures the Sweep Type and frequency range for IM Spectrum measurements.

Sweep Type

Provides several methods to tune the IM Spectrum receivers (NOT stimulus) to view the power spectrum of arbitrary frequency ranges or various distortion products.

Linear   Allows the start/stop or center/span receiver frequencies to be set arbitrarily for f1 and f2.  Enter the Response Settings below.

2nd Order  Couples the receiver frequency range to f1 and f2 to provide a convenient means of observing the spectrum surrounding ONLY the high-side 2nd order harmonic where Center = (f1 + f2), Span = 3 * (f2 – f1). Note: The center frequency is NOT set on the main tones.

3rd Order   Couples receiver frequency range to f1 and f2 to provide a convenient means of observing the spectrum surround the main-tones including the 3rd Order products where Center = (f1 + f2) / 2, Span = 4 * (f2 – f1).

Nth Order  Couples receiver frequency range to f1 and f2, providing a convenient means of observing the spectrum surrounding the main-tones for an arbitrary span where Center = (f1 + f2) / 2, and Span = N * (f2 – f1). This allows you to set the span arbitrarily, but have the center frequency track the main tone frequencies.

Resolution BW

The IM Spectrum channel utilizes a set of Gaussian filters instead of the standard VNA IF filters in order to provide similar behavior to traditional spectrum analyzers.

The comprehensive list of filters that are available for IM spectrum are: 3 MHz, 1 MHz, 600 kHz, 300 kHz, 150 kHz, 100 kHz, 60 kHz, 10 kHz, 3 kHz, and 1 kHz.

Note: The 10 kHz Res BW filter can generate image signals which are not a product of the DUT.  You can verify the integrity of a questionable signal by switching to the 3 kHz or 60 kHz filter and looking for the image signal in the same location.

Not all of these filters are available for all measurements. Narrower filters are available for use with narrower frequency spans, and wider filters are available for wider spans.

Stimulus Settings

Allows configuration of the main-tone frequencies. Available ONLY when Tracking is OFF.

  • fc (main-tone center frequency)  = (f1 + f2) / 2

  • DeltaF (main-tone frequency separation) = (f2 – f1).

  • f1  = Low-side main-tone frequency

  • f2  = High-side main-tone frequency

Response Settings

Allows configuration of the frequency range to sweep the receivers in terms of start/stop or center/span. Available for Linear sweep types ONLY.

  • Start Spectrum = first frequency point of the power spectrum sweep

Note: The minimum Start Spectrum frequency that can be set is 40 MHz.

  • Stop Spectrum = last frequency point of the power spectrum sweep

  • Center Spectrum = (Start Spectrum + Stop Spectrum) / 2

  • Span Spectrum = (Stop Spectrum – Start Spectrum)

 

Power tab - IM Spectrum -dialog box help

Learn about this dialog

 

Tracking tab - IM Spectrum -dialog box help

These selections are NOT available when there is no Swept IMD channel.

Allows the IM Spectrum channel to use (track) the stimulus (Main Tone) settings of an existing Swept IMD channel.

Tracking Enable  Check to use the frequency and power stimulus settings from the specified IMD channel. When enabled, stimulus settings on the Frequency Tab are disabled and ALL stimulus settings, such as frequencies, power and attenuator settings, and calibration, are copied from the Swept IMD channel to the IM Spectrum channel.

IM Spectrum trace (bottom) tracking with Swept IMD traces (top)

  • In the top Swept IMD window the main tones are swept from 4 GHz to 6 GHz with some specified delta F tone separation. The marker is on the center data point at 5 GHz.

  • The bottom IM Spectrum window center frequency is the same as the above marker: 5 GHz, but it has a much narrower frequency range of +/- 500 kHz. The IM Spectrum channel sets the receiver to see the two main tones, plus the third, fifth, and seventh-order products.

Step Mode

When tracking is enabled, set the method by which the IM spectrum measurement tracks the IMD channel.

Manual Step  When selected, IM Spectrum measurements occur at only the specified IMD channel data point. Stimulus Point specifies the data point, by number, in the Swept IMD channel which has the stimulus settings to use for the IM Spectrum sweep.

Automatic Step  When selected, causes the IM Spectrum channel to sequentially setup each of the stimulus conditions through which the Swept IMD channel sweeps the DUT. Each sweep of IM Spectrum is performed using the next set of stimulus conditions.

For example, in the above image, the first Swept IMD data point is at 4 GHz. The first IM Spectrum sweep uses a center frequency of 4 GHz. The following IM Spectrum sweep would be at the second Swept IMD data point or 4.01 GHz, and so forth. After the last data point in the sweep is reached, the IM Spectrum channel begins again at the first Swept IMD data point. The only indication that Tracking is enabled is in Automatic mode, you can see the center frequency increment with each IM Spectrum sweep.

 

 

Configure tab- IM Spectrum Setup -dialog box help

To accommodate single-source VNA models, an external source can be used for the RF2 tone.

Learn how to configure an external source and combiner to make Swept IMD, IMDx, IM Spectrum, and IM Spectrum for Converters measurements.

RF1  Always uses VNA internal source 1.

RF2  Available for selection when an external source is configured and Active.

Add Source  Click to configure an external source using the External Source Configuration dialog.

Path Configuration  Click to launch the Path Configuration dialog (PNA-X models only).

Calibration

A calibration corrects the IM Spectrum source and receiver power level accuracy of the displayed Tones.

A calibration of the IM Spectrum channel is NOT performed using the Calibration wizard. An IM Spectrum channel is calibrated by applying a Cal Set in one of the following ways:

See Swept IMD Calibration