This example uses the following interfaces to perform a power calibration using two power sensors.
Learn more about Reading and Writing Calibration data using COM.
This VBScript (*.vbs) program can be run as a macro in the VNA. To do this, copy the following code into a text editor file such as Notepad and save on the VNA hard drive as Calibrate.vbs. Learn how to setup and run the macro.
See Other COM Example Programs
set app = CreateObject("Agilentpna835x.application") app.Reset app.CreateMeasurement 1, "S11", 0, -1 ' create default S11 parameter app.ActiveChannel.StartFrequency = 1e9 app.ActiveChannel.StopFrequency = 2e9 set calMgr = app.GetCalManager() set guidedCal = calMgr.GuidedCalibration guidedCal.Initialize 1, false guidedCal.ConnectorType(1)="APC 3.5 male" guidedCal.ConnectorType(2)= "APC 3.5 female" guidedCal.CalKitType(1)= "N4691-60004 ECal" guidedCal.CalKitType(2)="N4691-60004 ECal" guidedCal.PerformPowerCalibration(2)= true set sensors = guidedCal.GuidedCalibrationPowerSensors(2) sensors.UseMultipleSensors = true sensors.Item(1).Name = "pmar1" sensors.Item(1).StartFrequency = 1e9 sensors.Item(1).StopFrequency = 1.5e9 sensors.Add "pmar2" sensors.Item(2).StartFrequency = 1.5e9 sensors.Item(2).StopFrequency = 2e9 numSteps = guidedCal.GenerateSteps() for i = 0 to numSteps-1 desc = guidedCal.GetStepDescription(i + 1) msgbox desc guidedCal.AcquireStep(i + 1) next guidedCal.GenerateErrorTerms() |