Contains the methods and properties used to perform a Guided Calibration.
|
Important! Do NOT use commands from the Calibrator (Unguided calibration) object when performing a Guided calibration. Use ONLY the GuidedCalibration object. The ONLY exception is: Use OrientECalModule_Property and ECalPortMapEx_Property on the Calibrator Object to specify orientation for both guided and unguided calibrations. |
A Guided Calibration must be performed on the Active Channel. To activate a channel, activate any measurement on that channel. Do this using meas.Activate, which requires you already have a handle to the measurement.
For standard S-parameter channels:
Dim app as AgilentPNA835x.Application
Dim CalMgr
Set CalMgr = App.GetCalManager
Dim guidedCal
Set guidedCal = CalMgr.GuidedCalibration
To calibrate an Application channel, see CreateCustomCalEx Method.
THRU Pairs sequenceThe Smart/Guided Cal logic always determines the best calibration based on your specified connectors and ports. The following three commands overwrite the SmartCal logic. Send these commands ONLY if you have a deliberate reason for overwriting the SmartCal logic. When sending one or more of these commands, they must be sent in the following sequence with the other commands listed here. Note: The Initialize command is sent before and after these three commands.
|
Methods |
|
Description |
|---|---|---|
|
IGuidedCalibration |
Acquire data for a cal step. |
|
|
IGuidedCalibration2 |
Apply a cal as Delta Match Cal. |
|
|
IGuidedCalibration |
Generates the error terms for the calibration. |
|
|
IGuidedCalibration2 |
Initiates a global delta match calibration. |
|
|
IGuidedCalibration |
Request to generate a connection list and return the number of steps required. |
|
|
IGuidedCalibration5 |
Returns the list of cal kits for the connector type. |
|
|
IGuidedCalibration3 |
Gets the list of port pairings for which isolation standards will be measured during calibration. |
|
|
IGuidedCalibration |
Query description of a step. |
|
|
IGuidedCalibration |
Initial setup with channel context for the remote cal object. |
|
|
IGuidedCalibration10 |
Resets the specified guided cal connection step as unmeasured. |
|
|
IGuidedCalibration3 |
Sets the list of port pairings for which isolation standards will be measured during calibration. |
|
|
IGuidedCalibration4 |
Show the Cal Window, or custom Cal Window, before acquiring a Cal standard. |
|
Properties |
Interface |
Description |
|
IGuidedCalibration |
Sets the cal kit for the port. |
|
|
IGuidedCalibration |
Superseded with GetCompatibleCalKits Method |
|
|
IGuidedCalibration |
Sets the connector type for the port. |
|
|
IGuidedCalibration4 |
Provides access to additional Properties and Methods which extends the GuidedCal Object. |
|
|
IGuidedCalibration3 |
Value by which to increment the channel's averaging factor during measurement of isolation standards. |
|
|
IGuidedCalibration10 |
Returns the number of iterative measurement acquisitions that has been made for the specified step. |
|
|
IGuidedCalibration10 |
Returns the minimum number of required iterative measurement acquisitions for the specified step. |
|
|
IGuidedCalibration3 |
Specifies the calibration method for each port pair. |
|
|
IGuidedCalibration3 |
Specifies the calibration THRU method for each port pair. |
|
|
IGuidedCalibration7 |
Perform Guided Power Cal. |
|
|
IGuidedCalibration2 |
Returns port numbers that need delta match cal. |
|
|
IGuidedCalibration6 |
Sets power level for power cal in several applications. |
|
|
IGuidedCalibration6 |
Sets Cal Kit for power cal in several applications. |
|
|
IGuidedCalibration6 |
Sets Power sensor connector for power cal in several applications. |
|
|
IGuidedCalibration9 |
Loads a file that defines a power table. |
|
|
IGuidedCalibration10 |
Specifies the behavior for guided cal steps that involve a sliding load. |
|
|
IGuidedCalibration |
Superseded with PathCalMethod and PathThruMethod |
|
|
IGuidedCalibration |
Sets the thru connection port pairs. |
|
|
IGuidedCalibration11 |
Enables Dynamic Uncertainty. |
|
|
IGuidedCalibration |
Obsolete - Use Custom Cal Window commands. |
|
|
IGuidedCalibration |
Gets Valid Connector Types. |
|
Interface |
Introduced with VNA Rev: |
|
IGuidedCalibration |
5.0 |
|
IGuidedCalibration2 |
5.25 |
|
IGuidedCalibration3 |
7.11 |
|
IGuidedCalibration4 |
8.0 |
|
IGuidedCalibration5 |
9.0 |
|
IGuidedCalibration6 |
9.10 |
|
IGuidedCalibration7 |
9.30 |
|
IGuidedCalibration8 |
|
|
IGuidedCalibration9 |
9.42 |
|
IGuidedCalibration10 |
9.85 |
|
IGuidedCalibration11 |
10.40 |