Write-only |
About Source Power Cal |
Description |
This command is replaced with AcquirePowerReadingsEx Method Initiates a source power cal acquisition. |
VB Syntax |
powerCalibrator.AcquirePowerReadings device [,sync] |
Variable |
(Type) - Description |
|
powerCalibrator |
(object) - A SourcePowerCalibrator object |
|
device
|
(enum NAPowerAcquisitionDevice) The specific device (sensor on the power meter) to be used for the acquisition. Choose from: 0 – naPowerSensor_A 1 – naPowerSensor_B To use the sensor that currently corresponds to the frequency of interest, use the value from the PowerAcquisitionDevice property. |
|
sync
|
(boolean) Optional argument. If not specified, value is set to False. Choose from: True (1) – The method does not return until this acquisition has completed (the program calling this method is halted while waiting for the method to return). False (0) – The method initiates an acquisition then returns immediately (while the acquisition still proceeds). The program calling this method can then perform other operations during the acquisition. |
Return Type |
None |
Default |
Not Applicable |
Examples |
powerCalibrator.AcquirePowerReadings naPowerSensor_A, True |
C++ Syntax |
HRESULT AcquirePowerReadings(tagNAPowerAcquisitionDevice enumAcqDevice, VARIANT_BOOL bSync); |
Interface |
ISourcePowerCalibrator |