Write-only |
|
Description |
Acquire the measurement data for the specified step in the calibration process. For an ECal User characterization this measures the ECal module. Note: Guided Cal allows you to measure standards in any order. See an example. |
VB Syntax |
obj.AcquireStep (n) |
Variable |
(Type) - Description |
|
obj |
Any of the following: GuidedCalibration (object) SMCType (object) VMCType (object) ECalUserCharacterizer (object) - Currently, only ONE step is required to measure the ECal module. |
|
n
|
Step number in the calibration process. Use GenerateSteps to determine the total number of steps. Use GetStepDescription to read the description of each step. |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
VMC.AcquireStep (3) |
C++ Syntax |
HRESULT put_AcquireStep(long step); |
Interface |
SMCType VMCType IGuidedCalibration IECalUserCharacterizer |