Write-only |
About Source Power CalAbout PMAR |
Description |
Adds a PowerLossSegment to the PowerLossSegments collection. Also, Adds a PowerLossSegmentPMAR to the PowerLossSegmentsPMAR collection. To ensure predictable results, it is best to remove all segments before defining a new list of segments. For each segment in the collection, do a seg.Remove. Segments and values can also be added using the CharacterizeAdaptor Macro. |
VB Syntax |
segs.Add (item [ size]) |
Variable |
(Type) - Description |
|
segs |
A PowerLossSegments collection A PowerLossSegmentsPMAR collection. |
|
item |
(variant) - Number of the new segment. If it already exists, a new segment is inserted at the requested position. |
|
size |
(long integer) - Optional argument. The number of segments to add, starting with item. If unspecified, value is set to 1. Add up to 9999 segments. |
Return Type |
None |
Default |
Not Applicable |
Examples |
segs.Add 1, 4 'Adds segments 1,2,3 and 4 |
C++ Syntax |
HRESULT Add(VARIANT index, long size); |
Interface |
IPowerLossSegments |