Write-only |
About Source Power Cal |
Description |
This command replaces ApplyPowerCorrectionValues Method. Applies the array of power correction values to the channel memory and turns correction ON. Perform after completing a source power cal acquisition sweep. This command does NOT save the correction values. To save correction values, save an instrument / calibration state (*.cst file) after performing a source power cal. Optionally, as part of the source power calibration, perform calibration of the reference receiver used in the power calibration. Learn more. |
VB Syntax |
powerCalibrator.ApplyPowerCorrectionValuesEX [rRec] |
Variable |
(Type) - Description |
|
powerCalibrator |
(object) - A SourcePowerCalibrator object |
|
rRec |
(Enum as NASourcePowerApplyCorrectionOption) Optional argument. Choose from: 0 - naSourcePowerApplyCorrectionDefault Do NOT perform and save a calibration of the reference receiver. (Default if not specified). 1 - naIncludeReferenceReceiverPowerCal Perform and save a calibration of the reference receiver. The Cal Set, which includes only the reference receiver cal, is saved to the destination specified by RemoteCalStoragePreference. |
Return Type |
None |
Default |
Not Applicable |
Examples |
powerCalibrator.ApplyPowerCorrectionValuesEX powerCalibrator.ApplyPowerCorrectionValuesEX (naIncludeReferenceReceiverPowerCal) |
C++ Syntax |
HRESULT ApplyPowerCorrectionValuesEx(enum NASourcePowerApplyCorrectionOption option); |
Interface |
ISourcePowerCalibrator5 |