Write-only |
About Source Power Calibration |
Description |
Copies and applies an existing Source Power Calibration to another channel. |
VB Syntax |
chan.ApplySourcePowerCalibrationTo (fromPortNum, targetChan, targetPortNum); |
Variable |
(Type) - Description |
|
chan |
A Channel (object) |
|
fromPortNum |
(Long) Port number of the existing source power correction. |
|
targetChan |
(Long) Channel number to which the source power correction will be copied. |
|
targetPortNum |
(Long) Port number to which the source power correction will be applied. |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
chan.ApplySourcePowerCalibrationTo 1,2,1 |
C++ Syntax |
HRESULT ApplySourcePowerCalibrationTo (long fromPortNumber, long otherChannelNumber, long portNumber); |
Interface |
IChannel11 |