Write-only |
About ECal Orientation |
Description |
Returns the ECal port that is connected to the specified VNA port. A calibration does not have to be in process. |
VB Syntax |
ecalPortNumber = ecal.AutoOrient (chanNum, pnaPort, ecalCharNum) |
Variable |
(Type) - Description |
|
ecalPortNumber |
(Long) Variable to store the returned ECal port number that is connected to the specified VNA port number. The returned ECal port number is a 1-based number: 1 = Port A, 2 = Port B, 3 = Port C, 4 = Port D. Zero (0) is returned when the auto-orientation routine is unable to resolve the orientation. |
|
ecal |
A ECalModule Object (object) |
|
chanNum |
(Long) Channel number that contains the frequency range that will be calibrated. |
|
PNAPort |
(Long) VNA port number. |
|
ecalCharNum |
(Long) User Characterization number that matches the physical adapters/fixtures that are on the ECal module. This aids in determining the orientation of the ECal module. Choose from: 0 Factory characterization (no adapters - data that was stored in the ECal module by Keysight) 1 User characterization #1 2 User characterization #2 ...and so forth up to: 12 User characterization #12 |
Return Type |
Long Integer |
Default |
Not Applicable |
Examples |
Dim app As AgilentPNA835x.Application Set app = CreateObject("AgilentPNA835x.Application", <analyzerName>) Dim pna pna.Preset Const chanNum = 1 pna.Channels(chanNum).StopFrequency = 20E9 ' for a 20 GHz ECal mod Const pnaPortNumber = 1 Const ecalCharacterizationNum = 0 Dim calMgr Set calMgr = pna.GetCalManager Dim ecalPortNumber ' The returned ECal port number is a 1-based number ' (1 = Port A, 2 = Port B, etc) ecalPortNumber = calMgr.ECalModules(1).AutoOrient(chanNum, pnaPortNumber, ecalCharacterizationNum) MsgBox "ECal port number attached to PNA port 1 = " & ecalPortNumber |
C++ Syntax |
HRESULT AutoOrient( long channel, long pnaPortNumber, long characterization, long *pECalPortNumber); |
Interface |
IECalModule |