Allows access to ECal modules that are connected to the VNA.
Get a handle to a ECalModule object by using the ECalModules collection. This is done through the CalManager object with the app.GetCalManager Method.
|
Dim app As AgilentPNA835x.Application Set app = CreateObject("AgilentPNA835x.Application", <analyzerName>) Dim pna pna.Preset Const chanNum = 1 pna.Channels(chanNum).StopFrequency = 20E9 ' for a 20 GHz ECal mod Const pnaPortNumber = 1 Const ecalCharacterizationNum = 0 Dim calMgr Set calMgr = pna.GetCalManager Dim ecalPortNumber ' The returned ECal port number is a 1-based number ' (1 = Port A, 2 = Port B, etc) ecalPortNumber = calMgr.ECalModules(1).AutoOrient(chanNum, pnaPortNumber, ecalCharacterizationNum) MsgBox "ECal port number attached to PNA port 1 = " & ecalPortNumber |
Methods |
Interface |
Description |
|---|---|---|
|
IECalModule |
Returns the orientation (which ECal port is connected to which VNA port) outside of the context of a calibration. |
|
Properties |
|
Description |
|
None |
|
|
|
Interface |
Introduced with VNA Rev: |
|
IECalModule |
8.50 |