Write-only |
About Cal Window |
Description |
Clears the flags for windows to be shown during calibrations other than the Cal Window. To flag a window to be shown see DisplayNAWindowDuringCalAcquisition |
VB Syntax |
calMgr.DisplayOnlyCalWindowDuringCalAcquisition |
Variable |
(Type) - Description |
|
calMgr |
(object) - A CalManager object |
Return Type |
Not Applicable |
Default |
Not Applicable |
Example |
calMgr.DisplayOnlyCalWindowDuringCalAcquisition |
C++ Syntax |
HRESULT DisplayOnlyCalWindowDuringCalAcquisition() |
Interface |
ICalManager5 |