Write-only |
About Frequency Span |
Description |
Sets the frequency span to the entire frequency span of the analyzer. |
VB Syntax |
chan.FrequencySpanFull |
Variable |
(Type) - Description |
|
chan |
(object) - A Channel object |
Return Type |
None |
Default |
Maximum frequency span of the analyzer |
Examples |
chan.FrequencySpanFull |
C++ Syntax |
HRESULT FrequencySpanFull ( ); |
Interface |
IChannel25 |