Description |
Note: This property is replaced by GetECALModuleInfoEx Method Returns the following information about the connected ECAL module: model number, serial number, connector type, calibration date, min and max frequency. The characterization within the ECal module that this information will be read from is specified by the ECALCharacterization property on the ICalibrator2 interface. The default value of the ECALCharacterization property is naECALFactoryCharacterization. |
VB Syntax |
moduleInfo = cal.GetECALModuleInfo (module) |
Variable |
(Type) - Description |
|
moduleInfo |
(string) - variable to store the module information |
|
cal |
A Calibrator (object) |
|
module |
(enum NAECALModule) – ECAL module. Choose from: 0 - naECALModule_A 1 - naECALModule_B |
Return Type |
String |
Default |
Not Applicable |
Examples |
info = cal.GetECALModuleInfo(naECALModule_A) Example return string: ModelNumber: 85092-60007, SerialNumber: 01386, ConnectorType: N5FN5F, PortAConnector: Type N (50) female, PortBConnector: Type N (50) female, MinFreq: 30000, MaxFreq: 9100000000, NumberOfPoints: 250, Calibrated: July 4 2002 |
C++ Syntax |
HRESULT GetECALModuleInfo(tagNAECALModule ecalModule, BSTR* info); |
Interface |
ICalibrator |