Read-only |
Data Access Map |
Description |
Retrieves complex data from the specified location. |
VB Syntax |
measData.getNAComplex location, numPts, data |
Variable |
(Type) - Description |
|
measData |
An IArrayTransfer interface which supports the Measurement object |
|
location |
(enum NADataStore) - Where the data you want is residing. Choose from: 0 - naRawData 1 - naCorrectedData 2 - naMeasResult 3 - naRawMemory 4 - naMemoryResult 5 - naDivisor - When reading data from, or writing data to, the normalization divisor, you must first create a divisor trace using DataToDivisor Method. |
|
numPts |
(long integer) - Number of data points requested |
|
data |
(NAComplex) - A one-dimensional array of NaComplex to store the data. |
Return Type |
NAComplex |
Default |
Not Applicable |
Examples |
Dim dComplex(201) AS NaComplex |
|
Notes |
The data is stored as Real and Imaginary (Re and Im) members of the NaComplex user defined type. You can access each number individually by iterating through the array. For i = 0 to NumPts-1 |
C++ Syntax |
HRESULT getNAComplex(tagNADataStore DataStore, long* pNumValues, TsComplex* pComplex) |
Interface |
IArrayTransfer |