Write only |
About ECal User Characterization |
Description |
Note: This command is replaced with InitializeEx Method Initiates a User Characterization of an ECal module. The specified channel number must be an S-parameter measurement channel. The User characterization number must already be set before issuing this command using CharacterizationNumber Property. |
VB Syntax |
userChar.Initialize (chan) |
Variable |
(Type) - Description |
|
userChar |
ECalUserCharacterizer (object) |
chan |
(Long) Channel number of a calibrated S-parameter channel. |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
userchar.Initialize(2) |
C++ Syntax |
HRESULT put_Initialize(long chanNum); |
Interface |
IECalUserCharacterizer |