Write / Read |
About ECal User Characterization |
Description |
Sets and reads the number to which the user characterization will be stored in the ECal module. The number must be set before sending Initialize or the default value (1) will be used.
|
VB Syntax |
userChar.CharacterizationNumber = value |
Variable |
(Type) - Description |
|
userChar |
An ECalUserCharacterizer Object |
|
value |
(Long) User Characterization number. Choose a value between 1 and 12. |
Return Type |
Long Integer |
Default |
Not Applicable |
Examples |
userChar.CharacterizationNumber = 5 |
C++ Syntax |
HRESULT put_CharacterizationNumber(long *Number); |
Interface |
IECalUserCharacterizer |