Write-only |
About Cal Sets |
Description |
This command is replaced with PutStandardComplexByString Puts standards acquisition data into the Cal Set. Learn more about Reading and Writing Cal Data |
|||||||||||||||||||
VB Syntax |
ICalData2.putStandardComplex class, rcv, src, numPts,real(),imag() |
|||||||||||||||||||
Variable |
(Type) - Description |
|||||||||||||||||||
|
ICalData2 |
An ICalData2 pointer to the Cal Set object |
|||||||||||||||||||
|
class |
(enum NACalClass) Standard. Choose from:
|
|||||||||||||||||||
|
rcv |
(long) - Receiver Port |
|||||||||||||||||||
|
src |
(long) - Source Port |
|||||||||||||||||||
|
numPts |
(long) - The number of data points in the real and imaginary arrays. |
|||||||||||||||||||
|
real() |
(single) - one-dimensional array containing the real part of the acquisition data. (0:points-1) |
|||||||||||||||||||
|
imag() |
(single) - one-dimensional array containing the imaginary part of the acquisition data. (0:points-1) |
|||||||||||||||||||
Return Type |
Not Applicable |
|||||||||||||||||||
Default |
Not Applicable |
|||||||||||||||||||
Examples |
Dim sdata As ICalData2 |
|||||||||||||||||||
C++ Syntax |
HRESULT putStandardComplex(tagNACalClass stdclass, long ReceivePort, long SourcePort, long lNumValues, float* pReal, float* pImag) |
|||||||||||||||||||
Interface |
ICalData2 |