Write-only |
About Balanced Measurements |
Description |
Maps the physical VNA ports to a device of balanced and single-ended logical ports for multi-port systems with greater than 4 ports. The device type is set using the following commands:
The Parameter command returns the list of parameters available for the currently selected topology. |
VB Syntax |
balTopology.SetCustomDUTTopology (portTypeSequence, physicalPortsSequence) |
Variable |
(Type) - Description |
|
balTopology |
A BalancedTopology (object) |
|
portTypeSequence |
(String) Device type for the balanced measurement. ‘B’ means the Balanced port; ‘S’ means the Single-ended port. Choose from: B – 1 port balanced device (2 ports) BB – Balanced - Balanced device (4 ports) BS – Balanced - Single-ended device (3 ports) SB – Single-ended - Balanced device (3 ports) SSB – Single-ended - Single-ended - Balanced device (4 ports) |
physicalPortsSequence |
(Variant) Physical port numbers mapped to the logical ports, separated by ‘,’. ‘B’ (Balanced) requires 2 physical port numbers: <nPos>, <nNeg>. ‘S’ (Single-ended) requires 1 physical port number. |
Return Type |
Not applicable - To read port mappings, use the BalancedTopology properties. |
Default |
Not Applicable |
Examples |
'The following example sets up 8 physical ports into 6 logical ports: |
C++ Syntax |
HRESULT SetCustomDUTTopology(BSTR portTypeSequence, VARIANT physicalPortsSequence) |
Interface |
IBalancedTopology3 |