Write-only |
About the Handler IO Connector |
Description |
Writes a value to the specified port. Use the get_Port Method to read the settings from the "readable" ports (C, D, E). |
VB Syntax |
handlerIo.put_Port (port, value) |
Variable |
(Type) - Description |
|
handlerIo |
(object) - A HandlerIO object |
|
port |
(enum as NAMatHandlerPort) - port to put data into. Choose from: naPortA - (0) naPortB - (1) naPortC - (2) naPortD - (3) naPortE - (4) naPortF - (5) naPortG - (6) naPortH - (7) |
|
value |
The number of the data bits to set. The following table shows what the value represents: Note: When writing to port G, port C must be set to output mode |
|
|
Port |
Max allowable <num> |
MSB...........................................LSB |
|
|
|
A |
255 |
A7...A0 |
Write-only |
|
|
B |
255 |
B7...B0 |
Write-only |
|
|
C |
15 |
C3...C0 |
Read-Write |
|
|
D |
15 |
D3...D0 |
Read-Write |
|
|
E |
255 |
D3...D0 + C3...C0 |
Read-Write |
|
|
F |
65535 |
B7...B0 + A7...A0 |
Write-only |
|
|
G |
1048575 |
C3...C0 + B7...B0 + A7...A0 |
Write-only |
|
|
H |
16777215 |
D3...D0 + C3...C0 + B7...B0 + A7...A0 |
Write-only |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
handlerIo.put_Port(naPortB, 1) |
C++ Syntax |
HRESULT put_Port ( tagNAMatHandlerPort Port, VARIANT Data ); |
Interface |
IHWMaterialHandlerIO |