Write-only. |
About Source Power Cal |
Description |
Note: This method is replaced by PutSourcePowerCalDataScalarEx Method Inputs source power calibration data (as scalar values) to this channel for a specific source port. |
VB Syntax |
chandata.putSourcePowerCalDataScalar sourcePort, numValues, data |
Variable |
(Type) - Description |
|
chandata |
(interface) – – An ISourcePowerCalData interface pointing to a Channel (object) |
|
sourcePort |
(long integer) – The source port for which calibration data is being input. |
|
numValues |
(long integer) – Number of data values being input. Note: If this does not equal the current number of points on the channel, the calibration will not be valid. |
|
data |
(single) – Array of source power cal data being input. |
Return Type |
None |
Default |
Not Applicable |
Examples |
Dim chanData As ISourcePowerCalData |
C++ Syntax |
HRESULT putSourcePowerCalDataScalar(long sourcePort, long numValues, float *pVals); |
Interface |
ISourcePowerCalData |