Description
A collection object that provides a mechanism for iterating through the segments of a power sensor cal factor table. The Cal Factor table can contain up to 100 segments. This collection is used when the Power Meter is used as a Receiver.
Example: Create a PMAR Device and Measurement
Methods |
Description |
|---|---|
|
Adds a PowerSensorCalFactorSegmentPMAR object to the collection |
|
|
Use to get a handle to a PowerSensorCalFactorSegmentPMAR object in the collection. |
|
|
Removes an PowerSensorCalFactorSegmentPMAR object from the collection. |
|
Properties |
Description |
|
Returns the number of PowerSensorCalFactorSegmentPMAR objects in the collection. |
|
|
Returns a handle to the Parent object of this collection. |