Description
Contains the properties describing a segment of a power sensor cal factor table that is used with Power Meter as Receiver.
You can get a handle to one of these segments through CalFactorSegmentsPMAR.Item(n).
Example: Create a PMAR Device and Measurement
Methods |
|
|---|---|
None |
|
Properties |
Description |
The frequency (Hz) associated with this segment. |
|
The cal factor (%) associated with this segment. |
|
Returns the number of this segment. |
Interface |
Introduced with VNA Rev: |
IPowerSensorCalFactorSegment |
9.0 |