ALL methods and properties on the PortExtension Object are Superseded with the Fixturing Object.
Contains the methods and properties that control Port Extensions.
Dim app As AgilentPNA835x.Application
Set app = CreateObject("AgilentPNA835x.Application", <analyzerName>)
Dim PortExt As PortExtension
Set PortExt = app.PortExtension
Methods |
|
|---|---|
|
None |
|
Property |
Description |
|
Sets the Input A extension value. |
|
|
Sets the Input B extension value. |
|
|
Sets the Input C extension value. |
|
|
Sets the Port 1 extension value. |
|
|
Sets the Port 2 extension value. |
|
|
Sets the Port 3 extension value. |
|
|
Turns Port Extensions ON and OFF. |
|
Interface |
Introduced with VNA Rev: |
|
IPort Extension |
1.0 |