Description
A collection object that provides a mechanism for accessing the PowerMeterInterface objects.
The collection size is limited to one PowerMeterInterface object. By default, that PowerMeterInterface object refers to GPIB, and to the GPIB address that is currently set for the power meter on that VNA.
The power meter is specified by using the Path property.
Get a handle to a power meter object using the PowerMeterInterfaces collection.
|
Dim app As AgilentPNA835x.Application Set app = CreateObject("AgilentPNA835x.Application", <analyzerName>) Dim pwrMtrInterfaces As PowerMeterInterfaces Set pwrMtrInterfaces = app.SourcePowerCalibrator.PowerMeterInterfaces If pwrMtrInterfaces.Count > 0 Then Dim pwrMtrInterface As PowerMeterInterface Set pwrMtrInterface = pwrMtrInterfaces(1) pwrMtrInterface.Path = naUSB pwrMtrInterface.Locator = ”Agilent Technologies,U2000A,MY12345678” End If |
Methods |
|
|---|---|
|
Use to get a handle to a PowerMeterInterface object in the collection. |
|
Properties |
Description |
|
Returns the number of objects in the collection. |
|
|
Returns a handle to the SourcePowerCalibrator |
|
Interface |
Introduced with VNA Rev: |
|
IPowerMeterInterfaces |
7.50 |