SpectrumAnalyzerCoherence

Description

Controls the Spectrum Analyzer Application Coherence and modulation distortion settings.

Accessing the SpectrumAnalyzerCoherence object

CComPtr<ISpectrumAnalyzer4> SA;

CComPtr<ICoherenceSA> sacoherence;

SA->GetCoherence(&sacoherence);

Method

Interface

See History

Description

Property

Interface

Description

MultiToneDataDisplay

ICoherenceSA

Sets and returns the data display mode.

MultiToneEnable

ICoherenceSA

Enables/disables multitone image rejection.

MultiToneHarmonicRejection

ICoherenceSA

Sets and returns the multitone harmonic rejection.

MultiToneNyquistProtection

ICoherenceSA2

Sets and returns the Nyquist protection level.

MultiTonePeriod

ICoherenceSA

Sets and returns the multitone image rejection period.

MultiToneReference

ICoherenceSA

Sets and returns the multitone image rejection offset frequency.

MultiToneSettingsValid

ICoherenceSA2

Returns the current multitone settings and determine if they are valid or not.

MultiToneSpacing

ICoherenceSA

Sets and returns the tone spacing of the multitone signal.

PhaseDisplayMinLevel

ICoherenceSA2

Sets and returns the phase display minimum level.

PhaseProcessState

ICoherenceSA2

Enables/disables phase computing.

VectorAverageEnable

ICoherenceSA

Sets and returns the ON/OFF state of the vector averaging.

VectorAverageValue

ICoherenceSA

Sets and returns the vector averaging value.

VectorAverageValueMax

ICoherenceSA

Returns the current maximum available vector averaging value.

SpectrumAnalyzerCoherence History

Interface

Introduced with VNA Rev:

ICoherenceSA

12.80

ICoherenceSA2

12.90