Write/Read |
About Vector Averaging |
Description |
Set and read the vector averaging value. |
VB Syntax |
sa.coherence.VectorAverageValue = value |
Variable |
(Type) - Description |
|
sa.coherence |
A SpectrumAnalyzerCoherence (object) |
|
value |
(Double) Choose a value between 0 and 65536. |
Return Type |
Double |
Default |
1 (no averaging) |
Examples |
sa.coherence.VectorAverageValue = 1 Write |
|
value = sa.coherence.VectorAverageValue 'Read |
|
C++ Syntax |
HRESULT put_VectorAverageValue(double val); HRESULT get_VectorAverageValue(double* val); |
Interface |
ICoherenceSA |