Write/Read |
About External Devices |
Description |
Set and return the state of activation of the device. When extDev.IOEnable = True, and this command is set to True, the VNA will attempt communication with the external device. An error is returned if communication cannot be verified. Note: Send this command AFTER sending other External Device settings to avoid communicating with the device before it has been fully configured. See Also ExternalDeviceDeActivatePolicy Property - Determines whether External Devices remain activated or are de-activated when the VNA is Preset or when a Instrument State is recalled. |
VB Syntax |
extDevices.Active = value |
Variable |
(Type) - Description |
|
extDevices |
An ExternalDevice (object) |
|
value |
(Boolean) Choose from: True - Device is active. False - Device is NOT active. |
Return Type |
Boolean |
Default |
False - When configured using the front panel user interface, the device is ON (activated) by default. |
Examples |
extDevices.Active = True 'Write bool = extDevices.Active 'Read See example program to configure PMAR device See example program to configure External Source |
C++ Syntax |
HRESULT get_Active( VARIANT_BOOL* value); HRESULT put_Active( VARIANT_BOOL newVal); |
Interface |
IExternalDevices |