Write/Read |
About External Devices |
Description |
Sets and returns whether an external device is enabled for IO communication with the VNA. When disabled (False), the VNA will NOT attempt to connect to the external device regardless of the instrument state (Active).property. Therefore, no errors will be produced if the device is not connected. This command is useful for debugging and testing states when the external device is not connected. This command is unnecessary in ordinary operation (when the device is connected). |
VB Syntax |
extDevices.IOEnable = value |
Variable |
(Type) - Description |
|
extDevices |
An ExternalDevice (object) |
|
value |
(Boolean) Choose from: True - Device is available for IO communication. False - Device is NOT available for IO communication. |
Return Type |
Boolean |
Default |
True |
Examples |
extDevices.IOEnable = True 'Write bool = extDevices.IOEnable 'Read See example program to configure PMAR device See example program to configure External Source |
C++ Syntax |
HRESULT get_IOEnable( VARIANT_BOOL* value); HRESULT put_IOEnable( VARIANT_BOOL newVal); |
Interface |
IExternalDevices |