Write/Read |
About SA Application |
Description |
Set and read the default values for DFT bandwidth. |
VB Syntax |
sa.dft.AutoBandwidth = value |
Variable |
(Type) - Description |
|
sa.dft |
A SpectrumAnalyzerDFT (object) |
|
value |
(Boolean) Choose from: 0 - OFF - DFT minimum and maximum values are set manually: Narrow - 500 kHz to 11 MHz Wide - 500 kHz to 44 MHz 1 - ON - DFT minimum and maximum values are set to their default values: Narrow - 1 MHz to 10 MHz Wide - 1 MHz to 34 MHz |
Return Type |
Boolean |
Default |
1 |
Examples |
sa.dft.AutoBandwidth = 0 'Write |
|
bwidth = sa.dft.AutoBandwidth 'Read |
|
C++ Syntax |
HRESULT put_AutoBandwidth(VARIANT_BOOL bEnable); HRESULT get_AutoBandwidth(VARIANT_BOOL* bEnable); |
Interface |
ISpectrumAnalyzerDFT |