SpectrumAnalyzerDFT Object


Description

Controls the Spectrum Analyzer Application Discrete Fourier Transform (DFT) settings.

Accessing the SpectrumAnalyzer object

CComPtr<ISpectrumAnalyzer4> SA;

CComPtr<ISpectrumAnalyzerDFT> sadft;

SA->GetDFT(&sadft);

 

Method

Interface

See History

Description

None

 

 

Property

Interface

Description

AutoBandwidth

ISpectrumAnalyzerDFT

Sets default values for DFT bandwidth.

BandwidthNarrowMax

ISpectrumAnalyzerDFT

Sets maximum value for narrow DFT bandwidth.

BandwidthNarrowMin

ISpectrumAnalyzerDFT

Sets minimum value for narrow DFT bandwidth.

BandwidthWideMax

ISpectrumAnalyzerDFT

Sets maximum value for wide DFT bandwidth.

BandwidthWideMin

ISpectrumAnalyzerDFT

Sets minimum value for wide DFT bandwidth.

BinaryFileEnabled

ISpectrumAnalyzerDFT

Enables binary file output.

DataBinCount

ISpectrumAnalyzerDFT

Returns the number of DFT points processed across the total RF span.

DataByteSize

ISpectrumAnalyzerDFT

Returns the byte size.

DataByteSizeLOW

ISpectrumAnalyzerDFT

Returns the low part of the byte.

DataByteSizeHIGH

ISpectrumAnalyzerDFT

Returns the high part of the byte.

DataBytesPerBin

ISpectrumAnalyzerDFT

Returns the number of bytes per bin.

DataExportMarkersEnabled

ISpectrumAnalyzerDFT2

Enables/disables adding marker data to the text file (*.txt) output.

DataExportWindowingFactor

ISpectrumAnalyzerDFT2

Returns the windowing factor for band power computation.

DataFirstRFBin

ISpectrumAnalyzerDFT

Returns the frequency of the first RF bin.

DataFormat

ISpectrumAnalyzerDFT

Sets and returns the data format.

DataLevelThreshold

ISpectrumAnalyzerDFT2

Sets and returns the threshold value (dBm).

DataLevelThresholdEnabled

ISpectrumAnalyzerDFT2

Enables/disables data level threshold mode.

ExportReceiverCount

ISpectrumAnalyzerDFT

Returns the number of exported receivers.

ExportReceiverList

ISpectrumAnalyzerDFT

Returns the currently exported receiver list.

ExportReceiverSetList

ISpectrumAnalyzerDFT

Sets and returns the list of exported receivers.

FIFOEnabled

ISpectrumAnalyzerDFT

Enables exporting data to the FIFO (First-IN, First-OUT) data buffer.

FileEraseEachSweep

ISpectrumAnalyzerDFT

Enables output data files to be erased after each sweep.

FilePrefix

ISpectrumAnalyzerDFT

Sets and returns the file name prefix and path of the data file.

FileVerboseEnabled

ISpectrumAnalyzerDFT

Enables output of data and frequency.

MemShareEnabled

ISpectrumAnalyzerDFT

Enables data to be output to shared memory.

MemShareName

ISpectrumAnalyzerDFT

Assigns a specified name to the shared data.

RecordSize

ISpectrumAnalyzerDFT

Returns the current DFT record size.

Resolution

ISpectrumAnalyzerDFT

Returns the DFT resolution.

TextFileEnabled

ISpectrumAnalyzerDFT

Enables text file output.

Type

ISpectrumAnalyzerDFT

Sets the DFT record size type.

 

SpectrumAnalyzerDFT History

Interface

Introduced with VNA Rev:

ISpectrumAnalyzerDFT

12.70 and 12.80

ISpectrumAnalyzerDFT2

13.25